990-5912C-001

Connect the Signal Cables for Galaxy VS UPS – Single System

NOTE: Route the signal cables separately from the power cables and route the Class 2/SELV cables separately from the non-Class 2/non-SELV cables.

GVSBPSU10K20H

GVSBPSU20K60H and GVSBPSU80K120H

  1. Connect the Class 2/SELV signal cables for the breaker indicator lights from the control terminal block in the maintenance bypass panel to the UPS as per your configuration.
    NOTE: The breaker indicator light circuit is considered Class 2/SELV. Class 2/SELV circuits must be isolated from the primary circuitry. Do not connect any circuit to the breaker indicator light terminals unless it can be confirmed that the circuit is Class 2/SELV.

    Single System – Single Mains

    Single System – Dual mains

  2. Connect the non-Class 2/non-SELV signal cables from the control terminal block in the maintenance bypass panel to the UPS as per your configuration.

    Single System – Single Mains

    Single System – Dual Mains

  3. Pull up the slack in the signal cables and fasten the signal cables to the cable reliefs.
QR code for this page

Was this helpful?