990-5912E-001

Connect the Signal Cables for Galaxy VS UPS – Simplified 1+1 Parallel System

NOTE: The disconnect device indicator lights are supplied by UPS 1 and will only work while UPS 1 is powered.
NOTE: The AUX switches are in optional parallel installation kit GVSOPT006 provided with the UPS.
NOTE: Route the signal cables separately from the power cables and route the Class 2/SELV cables separately from the non-Class 2/non-SELV cables.
  1. Install an AUX switch in the unit input disconnect device UIB/static switch input disconnect device SSIB and the maintenance bypass disconnect device MBB.
    1. Remove the AUX switch cover on the UIB/SSIB and MBB disconnect device.
    2. Install the AUX switch from kit GVSOPT006 in the UIB/SSIB and MBB disconnect device.
    3. Connect the non-Class 2/non-SELV signal cables to the AUX switch in the UIB/SSIB and MBB disconnect device.
    4. Reinstall the AUX switch cover on the UIB/SSIB and MBB disconnect device.
    5. Only for GVSBPSU80K120H: Fasten the signal cables to the plastic tabs to ensure correct separation from the busbars.

      GVSBPSU10K20H

      GVSBPSU20K60H

      GVSBPSU80K120H

  2. Connect the Class 2/SELV signal cables for the disconnect device indicator lights from the control terminal block in the maintenance bypass panel to the UPSs as per your configuration.
    NOTE: The disconnect device indicator light circuit is considered Class 2/SELV. Class 2/SELV circuits must be isolated from the primary circuitry. Do not connect any circuit to the disconnect device indicator light terminals unless it can be confirmed that the circuit is Class 2/SELV.

    Simplified 1+1 Parallel System – Single Mains

    Simplified 1+1 Parallel System – Dual mains

  3. On UPS 2: Cut the preinstalled jumper between pins 8 and 9 on the terminal connector for J6618 on board 640-4864.
    NOTICE
    Risk of incorrect equipment behavior
    Cut the preinstalled jumper between pins 8 and 9 on terminal J6618 on board 640-4864 on UPS 2. The 24 V_SELV_OUT cannot be supplied from both UPSs.
    Failure to follow these instructions can result in equipment damage.
  4. Connect the non-Class 2/non-SELV signal cables from the control terminal block in the maintenance bypass panel to the UPSs as per your configuration.

    Simplified 1+1 Parallel System – Single Mains

    Simplified 1+1 Parallel System – Dual Mains

    GVSBPSU10K20H

    GVSBPSU20K60H

    GVSBPSU80K120H

  5. Pull up the slack in the signal cables and fasten the signal cables to the cable reliefs.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.