990-91111G-001

Final Installation

  1. Reinstall the top cover:
    1. Tilt the top cover and slide it onto the UPS from the rear. Tabs in the rear of the top cover must connect to the slots in the rear of the UPS.
    2. Push the top cover down in the front.

      Rear View of the UPS

    3. Reinstall the screws.

      Front View of the UPS

  2. Check the fastening of the cable lugs.
    CAUTION
    Risk of equipment damage
    Check the fastening of the cable lugs. If the cable lugs move due to pulling on cables, the bolt can become loose.
    Failure to follow these instructions can result in injury or equipment damage.
  3. Reinstall the transparent cover.

    Front View of the UPS

  4. Reinstall the lower front plate.

    Front View of the UPS

  5. Only for seismic anchoring:
    1. Install the seismic front anchoring bracket on the UPS with the provided M8 bolts.
    2. Mount the seismic front anchoring bracket on the UPS to the floor. Use appropriate hardware for the floor type – the hole diameter in the front anchoring bracket is ø18 mm.

    Front View of the UPS

  6. Lower the front and rear leveling feet on the UPS with a wrench until they connect with the floor. Use a bubble-leveler to check that the UPS is level. This step is not necessary for a UPS with seismic anchoring.

    Front View of the UPS

    CAUTION
    Tip hazard
    Do not move the cabinet after the leveling feet have been lowered.
    Failure to follow these instructions can result in injury or equipment damage.
  7. Only for UL 924 and CSA C22.2 NO. 141-15 solutions: Fill out the label on the lower front plate with the UPS output rating in kW.
  8. Reinstall the front panel on the UPS:
    1. Insert the two tabs in the bottom of the front panel in the UPS at a tilted angle.
    2. Reconnect the front panel strap to the UPS.
    3. Close the front panel and lock with the two locking knobs.
QR code for this page

Was this helpful?