990-91111L-001

Connect the Signal Cables from a Modular Battery Cabinet

For installation with adjacent modular battery cabinet, use the signal cables provided in optional installation kit GVSOPT030. For installation with remote modular battery cabinets, signal cables are not provided. Follow the modular battery cabinet installation manual to prepare for installation.

  1. For a remote modular battery cabinet: Route the signal cables from modular battery cabinet 1 through the rear of the UPS.
  2. For an adjacent modular battery cabinet: Route the signal cables from modular battery cabinet 1 to the UPS as shown.
    1. Route the signal cables from modular battery cabinet 1 into the UPS through the opening.
    2. Route the signal cables up through the cable channel in the UPS.

    Front View of Adjacent Modular Battery Cabinet 1 and the UPS

  3. Connect the signal cables from modular battery cabinet 1 to the UPS:
    1. Mount a termination plug in J8008 on board 640-7552 in the last modular battery cabinet (T).
    2. Connect the signal cable from J8011 on board 640-7552 in modular battery cabinet 1 to J6619 and J6604 on board 640-4843 in the UPS.
    3. Connect the signal cable from J8007 on board 640-7552 in modular battery cabinet 1 to J6608 on board 640-4864 in the UPS.

    Signal Cable Connections between Four Modular Battery Cabinets and the UPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.