990-91111L-001

Installation Procedure for Parallel Marine Systems

Simplified 1+1 Parallel System

Parallel System

  1. Install the IP22 kit GVSOPT026 on the UPSs – follow the installation manual provided with the kit.
  2. Install the UPSs and the modular battery cabinet(s) (if present) on the mounting skid kit GVSOPT027 – follow the installation manual provided with the kit.
  3. Prepare for Installation.
  4. Install the Power Module(s).
  5. Install the Seismic Anchoring (Option).
  6. Connect the Power Cables
  7. Connect the Signal Cables.
  8. Connect the Signal Cables from a Modular Battery Cabinet.
  9. Connect the Signal Cables from Switchgear and Third-Party Auxiliary Products.
  10. Perform one of the following:
  11. Connect the PBUS Cables.
  12. Connect the External Communication Cables.
  13. Add Translated Safety Labels to Your Product.
  14. Final Installation.
For moving or decommissioning the UPS after installation has been completed, see Decommission or Move the UPS to a New Location.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?