990-91141L-001

Configuration Options

  • Compact design, high density technology, and modular architecture

  • Single or dual mains

  • Up to 4+0 UPSs in parallel for capacity

  • Up to 3+1 UPSs in parallel for redundancy

  • Default rear or bottom cable entry

  • ECO mode

  • eConversion mode

  • EcoStruxure IT compatible

  • Generator compatible

  • Touchscreen LCD

  • Replacement of power module in any operation mode (Live Swap)*

  • Halogen-free cables for marine-certified and scalable UPS models.

  • Supported battery types: VRLA, Lithium-ion, and NiCd.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.