990–5914A–001

Mount the Battery Breaker Box to the Wall

CAUTION
Risk of injury or equipment damage
  • Mount the battery breaker box to a wall or a rack that is structurally sound and able to support the weight of the unit.
  • Use appropriate hardware (not supplied) to mount the battery breaker box to the wall.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Four M10 x 30 torx and nuts are supplied for mounting the battery breaker box to a rack.

20–80 kW Battery Breaker Box

100–200 kW Battery Breaker Box

  1. Measure and mark the four mounting hole locations on the wall.
  2. Drill holes in each of the four marked locations.
  3. Loosen the three screws and open the inner door.

    Front View of the Battery Breaker Box

  4. Line up the battery breaker box with the four holes on the wall and mount the battery breaker box to the wall.
QR code for this page

Was this helpful?