990-5909C-001

Connect the Signal Cables

  1. Connect the provided Class 2/SELV signal cable 0W49283 to board 640-4864 in the UPS as shown.

    Single Mains System

    Dual Mains System

  2. Connect the non-Class 2/non-SELV signal cable 0W49284 to board 640-4843 in the UPS as shown.

    Single Mains System

    Dual Mains System

  3. Route the signal cables down through the cable channel in the right side of the UPS and into the maintenance bypass cabinet through the cable entry opening.
  4. Connect the signal cables at the cable connection point in the maintenance bypass cabinet.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.