990-5909C-001

Interconnect the UPS and the Maintenance Bypass Cabinet

  1. Reinstall the left upper side plate and the transparent plate on the maintenance bypass cabinet.

    Left Side View of the Maintenance Bypass Cabinet

  2. Only with conduit box: Reinstall the left lower side plate.
  3. Remove the transportation brackets from the maintenance bypass cabinet, if not already removed for seismic anchoring.
  4. Remove the three interconnection screws from the left side of the maintenance bypass cabinet. Save for interconnection.

    Front View of the UPS and the Maintenance Bypass Cabinet

  5. Position the UPS close to the maintenance bypass cabinet with a little free space between the cabinets.
  6. Push the UPS into place up against the maintenance bypass cabinet. The rear bracket on the maintenance bypass cabinet must connect to the UPS.

    Rear View of the Maintenance Bypass Cabinet and the UPS

  7. Install the three interconnection screws between the UPS and the maintenance bypass cabinet as shown.

    Front View of the UPS and the Maintenance Bypass Cabinet

  8. Lower the front and rear leveling feet on the UPS and the maintenance bypass cabinet with a wrench until they connect with the floor. Use a bubble-leveler to check that the UPS and maintenance bypass cabinet are level.

    Front View of the UPS

    CAUTION
    Risk of equipment damage
    Do not move the cabinet after the leveling feet have been lowered.
    Failure to follow these instructions can result in injury or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.