990-5909C-001

Install the Conduit Box

  1. Remove the middle rear plate on the maintenance bypass cabinet. Save the nuts for installing the conduit box.
  2. Remove the knockouts from the conduit box.
  3. Install the conduit box on the maintenance bypass cabinet with the nuts from step 1.
  4. Install the provided UPS input/UPS bypass cables 0W12758 and UPS output cables 0W12761 in the conduit box.
  5. Install the rear plate on the conduit box

    Rear View of the Maintenance Bypass Cabinet

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.