Decommission or Move the Maintenance Bypass Cabinet to a New Location
- Shut down the UPS system completely.
- Lockout/Tagout all breakers in the maintenance bypass cabinet and the upstream switchgear in the OFF (open) position.
- Lockout/Tagout all battery breakers in the switchgear/battery solution in the OFF (open) position.
- Remove the front panels from the maintenance bypass cabinet and the UPS.
- If present, Lockout/Tagout the backfeed breaker BF2 in the OFF (open) position on the UPS.
- Remove the lower and upper front plate from the maintenance
bypass cabinet.
DANGERHazard of electric shock, explosion, or arc flash- Do no remove any other plates or panels while there is power on the system.
- Before any work activity is started it must be confirmed with measurements directly on the terminals that no power is present.
Failure to follow these instructions will result in death or serious injury. - On the maintenance bypass cabinet, measure for and verify ABSENCE of voltage with a multimeter probe through the holes in the transparent plate for input/bypass and load.
- On the UPS, measure for and verify ABSENCE of voltage with
a multimeter probe on each busbar or terminal for input, bypass, output,
neutral, and DC. See UPS installation manual for details.
DANGERhAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASHMeasure for and verify ABSENCE of voltage on each busbar or terminal for input/bypass/output/neutral/DC busbar before continuing.Failure to follow these instructions will result in death or serious injury. - On the UPS, disconnect and remove the internal power cables coming from the maintenance bypass cabinet. See the UPS installation manual and Connect the Internal Power Cables for details. Save all parts for reinstallation.
- Remove the screws in the front that interconnect the UPS and the maintenance bypass cabinet externally. See Interconnect the UPS and the Maintenance Bypass Cabinet for details. Save all parts for reinstallation.
- On the UPS, disconnect and remove any signal cables from the UPS. See the UPS installation manual for details.
- If present, remove the seismic front anchoring bracket from the UPS and the maintenance bypass cabinet. Save for reinstallation.
- Reinstall the front panel on the UPS.
- Raise the feet of the UPS until the casters have full contact with the floor.
- Move the UPS out of the way of the maintenance bypass cabinet
by rolling it on the casters.
WARNINGTIPPING hazard- The casters of the UPS are exclusively for transport on flat, even, hard, and horizontal surfaces.
- The casters of the UPS are intended for transport over short distances (i.e. inside the same building).
- Move at a slow pace and pay close attention on the floor conditions and the balance of the UPS.
Failure to follow these instructions can result in death, serious injury, or equipment damage. - The maintenance bypass cabinet can tip over easily when
not interconnected with the UPS or mounted to the floor. Take appropriate
precautions to avoid the maintenance bypass cabinet tipping over.
If the original front transportation bracket is available and in undamaged
condition, install the front transportation bracket on the maintenance
bypass cabinet to increase stability.
WARNINGTipping hazardThe maintenance bypass cabinet can tip over easily when not interconnected with the UPS or mounted to the floor. Take appropriate precautions to avoid the maintenance bypass cabinet tipping over.Failure to follow these instructions can result in death, serious injury, or equipment damage. - Remove the right side panel from the maintenance bypass cabinet and reinstall the right side panel on the UPS. See Prepare the Maintenance Bypass Cabinet and the UPS for Cables for details.
- Remove the left side plates from the maintenance bypass cabinet.
- Measure for and verify ABSENCE of voltage
on each input/bypass/load/neutral/DC busbar in the maintenance bypass
cabinet before continuing.
DANGERhAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASHMeasure for and verify ABSENCE of voltage on each input/bypass/load/neutral/DC busbar before continuing.Failure to follow these instructions will result in death or serious injury. - Disconnect and remove the power cables from the maintenance bypass cabinet. See Connect the Power Cables in a 10-80 kW Top Cable Entry System, Connect the Power Cables in a 100-150 kW Top Cable Entry System, or Connect the Power Cables in a Bottom Cable Entry System for details.
- Disconnect and remove the signal cables from the maintenance bypass cabinet. See Connect the Signal Cables for details.
- Reinstall the left side plates on the maintenance bypass cabinet.
- Reinstall the front panel on the maintenance bypass cabinet.
- Raise the feet of the maintenance bypass cabinet until the casters have full contact with the floor.
- You can now move the maintenance bypass cabinet by rolling
it over the floor on the casters.
WARNINGTIPPING hazard- The casters of the maintenance bypass cabinet are exclusively for transport on flat, even, hard, and horizontal surfaces.
- The casters of the maintenance bypass cabinet are intended for transport over short distances (i.e. inside the same building).
- Move at a slow pace and pay close attention on the floor conditions and the balance of the maintenance bypass cabinet.
Failure to follow these instructions can result in death, serious injury, or equipment damage. - If present, remove the rear seismic anchoring bracket from the maintenance bypass cabinet and remove the seismic anchors from the floor. Save for reinstallation.
- The maintenance bypass cabinet can tip over easily when
not interconnected with the UPS or mounted to the floor. Take appropriate
precautions to avoid the maintenance bypass cabinet tipping over.
If the original rear transportation bracket is available and in undamaged
condition, install the rear transportation bracket on the maintenance
bypass cabinet to increase stability.
WARNINGTipping hazardThe maintenance bypass cabinet can tip over easily when not interconnected with the UPS or mounted to the floor. Take appropriate precautions to avoid the maintenance bypass cabinet tipping over during handling and preparation for transport/shipment.Failure to follow these instructions can result in death, serious injury, or equipment damage. - For transport over longer distances
or in conditions that are not suitable for the casters of the maintenance
bypass cabinet:
WARNINGTIPPING hazardFor transport over longer distances or in conditions that are not suitable for the casters of the maintenance bypass cabinet, ensure:- that personnel performing the transport have necessary skill and have received adequate training;
- to use appropriate tools to safely lift and transport the maintenance bypass cabinet;
- to protect the product against damage by using appropriate protection (like wrapping or packaging).
Failure to follow these instructions can result in death, serious injury, or equipment damage.Transportation requirements:
-
Mount the maintenance bypass cabinet in a vertical position in the center of a suitable pallet with minimum pallet dimensions: ? mm x ? mm. The pallet must be suitable for the weight of the maintenance bypass cabinet: 110-120 kg (243-265 lbs).
-
Use appropriate means of fixation to mount the maintenance bypass cabinet to the pallet.
-
The original shipping pallet in combination with the original transportation brackets can be reused, if in undamaged condition.
DANGERTIPPING hazard- The maintenance bypass cabinet must be appropriately fixed to the pallet immediately after being placed on the pallet.
- The fixation hardware must be strong enough to withstand vibrations and shocks during loading, transport, and unloading.
Failure to follow these instructions will result in death or serious injury.
WARNINGUnexpected equipment behaviorDo not lift the maintenance bypass cabinet with a forklift/pallet truck directly on the frame as it may bend or damage the frame.Failure to follow these instructions can result in death, serious injury, or equipment damage. - Perform
one of the following:
- Decommission the maintenance bypass cabinet, OR
- Move the maintenance bypass cabinet to a new location to install it.
- Only for installing the maintenance bypass cabinet in
a new location: Follow the installation manual to install the
maintenance bypass cabinet in the new location. See Installation Procedure for Top Cable Entry or Installation Procedure for Bottom Cable Entry for
installation overview. Startup must only be performed by Schneider
Electric.
DANGERhAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASHStartup must only be performed by Schneider Electric.Failure to follow these instructions will result in death or serious injury.