990-5909C-001

Final Installation

  1. Reinstall the upper and lower front plate.

    Front View of the Maintenance Bypass Cabinet

  2. Only for dual mains: Add the labels SSIB, HSSIB, and the diagram label on the upper front plate. The labels are provided with this manual.

    Front View of the Maintenance Bypass Cabinet – Single Mains

    Front View of the Maintenance Bypass Cabinet – Dual Mains

  3. Only for seismic anchoring:
    1. Install the seismic front anchoring bracket on the maintenance bypass cabinet with the provided M8 bolts.
    2. Mount the seismic front anchoring bracket on the maintenance bypass cabinet to the floor. Use appropriate hardware for the floor type – the hole diameter in the front anchoring bracket is ø18 mm.

    Front View of the Maintenance Bypass Cabinet

  4. Reinstall the front panel on the maintenance bypass cabinet:
    1. Insert the two taps in the bottom of the front panel in the maintenance bypass cabinet at a tilted angle.
    2. Reconnect the front panel strap to the maintenance bypass cabinet.
    3. Close the front panel and lock with the two locking knobs.

      Front Right View of the Maintenance Bypass Cabinet

  5. Follow the UPS installation manual to connect the internal power cables in the UPS.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.