990-91263A-001

Prepare for Installation

  1. Remove the front panel.
  2. Remove the upper plate.
  3. Remove the transparent plate.
  4. Remove the top cover.
  5. Remove side panels that will be adjacent to another modular battery cabinet or an adjacent UPS.
  6. Remove the cover from board 640-7552.
  7. Remove the battery cover.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.