990-91263-001

Connect the Power Cables for a UPS Rated for Maximum 50 kW

NOTICE
Risk of equipment damage
Only connect the DC cables from battery breaker to battery breaker in installations with a UPS rated for maximum 50 kW. For installations with a UPS rated over 50 kW, the DC cables from each modular battery cabinet must be connected directly in the UPS. See Connect the Power Cables for a UPS Rated over 50 kW.
Failure to follow these instructions can result in equipment damage.
  1. Connect the provided PE cable (0W49449) between the modular battery cabinets as shown.

    Front View of Two Modular Battery Cabinets

  2. Connect the provided DC cables (0W49426) between the modular battery cabinets as shown.

    Top View of the Modular Battery Cabinets

  3. For remote UPS:
    1. Connect the PE cable and the DC cables (not provided) in modular battery cabinet 1.
    2. Route the PE and DC cables out through the conduit box and into the UPS power cabling area.
    3. Follow the UPS installation manual to connect the PE and DC cables in the UPS.

    Front View of Modular Battery Cabinet 1 for Remote UPS

  4. For adjacent UPS with internal batteries:
    1. Connect the provided PE cable (0W49449) and DC cables (0W49426) in the UPS. Follow the UPS installation manual to connect and route the PE cable and DC cables in the UPS.
    2. Connect the PE and DC cables in modular battery cabinet 1.

    Front View of Modular Battery Cabinet 1 for Adjacent UPS

  5. For adjacent UPS for external batteries:
    1. Connect the PE cable (0W13065) and the DC cables (0W13071) from optional kit GVSOPT030 in modular battery cabinet 1.
    2. Route the PE and DC cables through the right side and into the UPS power cabling area.
    3. Follow the UPS installation manual to connect the PE and DC cables in the UPS.

    Front View of Modular Battery Cabinet 1 for Adjacent UPS

QR code for this page

Was this helpful?