Connect the Power Cables for a UPS Rated over 50 kW
| NOTICE |
|---|
|
Risk of equipment damage
For installations with a UPS rated over 50 kW, the DC cables from each modular battery
cabinet must be connected directly in the UPS.
Failure to follow these instructions can result in equipment damage.
|
- For remote UPS:
- Connect the PE cable and the DC cables (not provided) in each modular battery cabinet
- Route the PE and DC cables out through the conduit box and into the UPS power cabling area.
- Follow the UPS installation manual to connect the PE and DC cables in the UPS.
- For adjacent UPS for external batteries:
- Connect the provided PE cable (0W49449) between the modular battery cabinets as shown.
- Connect the PE cable from optional kit GVSOPT030 in modular battery cabinet 1 and route the PE cable through the right side and into the UPS power cabling area.
- Connect the DC cables from optional kit GVSOPT030 in each modular battery cabinet and route the DC cables through the right side and into the UPS power cabling area. The DC cables are routed through the modular battery cabinets.
- Follow the UPS installation manual to connect the PE and DC cables in the UPS.