990-91263A-001

Install the Seismic Anchoring (Option)

  1. Mount the rear anchor(s) to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchor is ø14 mm. Use the rear interconnection plate with multiple modular battery cabinets and/or an adjacent UPS.
  2. Install the rear anchoring bracket on the modular battery cabinet(s) with the provided M8 bolts.

    Rear View of the Modular Battery Cabinet

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.