990-91263A-001

Connect the Signal Cables

  1. Assign an ID to each modular battery cabinet with the switch below the battery breaker. Set the IDs according to the installation overview images in Installation Procedure for Adjacent Installation.

    Front View of the Modular Battery Cabinet

  2. Connect the provided signal cables between all the modular battery cabinets:
    1. Connect the provided signal cable 0W12680 from J8007 to J8008 on board 640-7552 between the modular battery cabinets.
    2. Connect the provided signal cable 0W76629 from J8011 to J8014 on board 640-7552 between the modular battery cabinets.
    3. Mount a termination plug (T) in the unused J8008 connector in the last modular battery cabinet.
    Modular Battery Cabinet 3 Modular Battery Cabinet 2 Modular Battery Cabinet 1

    Front View of Two Modular Battery Cabinets

  3. For installation with adjacent UPS with internal batteries:
    1. Connect the provided signal cable 0W12680 to J8007 on board 640-7552 in modular battery cabinet 1, route through the right side, and follow the UPS installation manual to connect the signal cables in the UPS.
    2. Connect the provided signal cable 0W76629 to J8011 on board 640-7552 in modular battery cabinet 1, route through the right side, and follow the UPS installation manual to connect the signal cables in the UPS.
  4. For installation with adjacent UPS for external batteries:
    1. Connect the signal cable 0W13069 from optional kit GVSOPT030 to J8007 on board 640-7552 in modular battery cabinet 1, route through the right side, and follow the UPS installation manual to connect the signal cables in the UPS.
    2. Connect the signal cable 0W13070 from optional kit GVSOPT030 to J8011 on board 640-7552 in modular battery cabinet 1, route through the right side, and follow the UPS installation manual to connect the signal cables in the UPS.

    Front View of Modular Battery Cabinet 1 for Adjacent UPS

  5. For remote installation:
    1. Connect signal cables to J8007 on board 640-7552 in modular battery cabinet 1, route through the rear, and follow the UPS installation manual to connect the signal cables in the UPS.
      NOTE: The provided signal cable 0W12680 is not long enough for a remote UPS installation. A 5 meter signal cable (0J-0W4527) or 50 meter signal cable (0J-0W3758) can be ordered from Schneider Electric. For other signal cable lengths, please contact Schneider Electric. This signal cable is classified as Class 2/SELV.
    2. Connect signal cables to J8011 on board 640-7552 in modular battery cabinet 1, route through the rear, and follow the UPS installation manual to connect the signal cables in the UPS.
      NOTE: The provided signal cable 0W76629 is not long enough for a remote UPS installation. Reuse the connectors from the provided signal cable 0W76629 to make new signal cables in the correct length. This signal cable is classified as non-Class 2/non-SELV.

      Signal Cable for UPS with Internal Batteries

      Signal Cable for UPS for External Batteries

    Rear View of Modular Battery Cabinet 1 for Remote UPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.