990-5909C-001

Maintenance Bypass Cabinet Weights and Dimensions

Commercial reference Weight kg (lbs) Height mm (in) Width mm (in) Depth mm (in)
GVSBPSU80G 110 (243) 1485 (58.46) 318 (12.52) 850 (33.46)
GVSBPSU150G 120 (265) 1485 (58.46) 318 (12.52) 850 (33.46)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?