990-5783L-001

Prepare the I/O Cabinet for Power Cables in Bottom Cable Entry Systems

DANGER
hazard of electric shock, explosion, or arc flash
Do not drill/punch holes for cables or conduits with the gland plates installed and do not drill/punch holes in close proximity to the UPS.
Failure to follow these instructions will result in death or serious injury.
  1. Loosen the bolts and remove the gland plates in the bottom of the I/O cabinet.

    Front View of the I/O Cabinet

  2. Drill or cut holes for cables/conduits in the bottom gland plate.
  3. Install conduits and reinstall the bottom gland plate.
    DANGER
    hazard of electric shock, explosion, or arc flash
    Ensure that there are no sharp edges that can damage the cables.
    Failure to follow these instructions will result in death or serious injury.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.