990-5783L-001

Position the Cabinets

DANGER
hazard of electric shock, explosion, or arc flash
Do not step/walk on top of the cabinets.
Failure to follow these instructions will result in death or serious injury.
NOTE: The cabinets must be moved to the final installation area individually and cannot be moved after they have been interconnected.
DANGER
hazard of electric shock, explosion, or arc flash
A minimum of one power cabinet and a maximum of four power cabinets must be placed on each side of the I/O cabinet.
Failure to follow these instructions will result in death or serious injury.
  1. Install the cover 0M-98993 from the installation kit on the right-most power cabinet.
  2. Install the interconnection cover 0M-82316 from the installation kit on the left-most power cabinet.
  3. Remove the side panels from the I/O cabinet and install them on the left side of the left-most power cabinet and on the right side of the right-most power cabinet.
    WARNING
    Hazard of arc flash
    • Do not make mechanical changes to the product (including removal of cabinet parts or drilling/cutting of holes) that are not described in the installation manual.
    • Move and install the indicated side panels in all installation types (including parallel installations with no air gap between the frames or in installations where the right-most power cabinet and/or the left-most power cabinet is placed against a wall).
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  4. Remove and dispose of the indicated transport bracket from the left side of the I/O cabinet.
  5. Remove and dispose of the indicated transport bracket from the right side of the I/O cabinet.
  6. Remove and dispose of the indicated transport bracket from the right side of the I/O cabinet.
  7. Remove the two metal plates from the I/O cabinet.
  8. Push the I/O cabinet into position against the rear anchoring bracket – the I/O cabinet will connect to the conic outcroppings on the rear anchoring bracket.
  9. Fasten the cabinet to the rear anchoring bracket with the two anchor bolts from the installation kit. Torque to 50 Nm (36.87 lb-ft).
  10. Push the power cabinets one by one into position against the rear anchoring brackets – the cabinets will connect to the conic outcroppings on the brackets.
    CAUTION
    risk of equipment damage
    When pushing the power cabinet into position, push on the frame to avoid damaging the signal cables.
    Failure to follow these instructions can result in injury or equipment damage.
  11. Fasten the cabinets to the rear anchoring brackets by tightening the bolts on the front of the cabinets. Torque to 50 Nm (36.87 lb-ft).
  12. Lower the two front feet on all cabinets until they connect with the floor – use a bubble-leveler to ensure that the cabinets are level. Use the provided levelling shims if necessary.
  13. Install the top baying brackets on the top of the cabinets and fasten with the provided screws.

    Front View of the I/O Cabinet and Two Power Cabinets

  14. Remove the three indicated plates in the left side of the I/O cabinet.
  15. Remove the two indicated plates in the left side of the I/O cabinet.
  16. Mount the M6 screws from the installation kit from right to left in the four marked locations between the I/O cabinet and the power cabinet placed to the left of the I/O cabinet.

    From the Power Cabinet on the Left Side of the I/O Cabinet to the I/O Cabinet

  17. Mount the M6 screws from the installation kit from right to left to tighten the cabinets together:
    • in the five marked positions between the power cabinets.

    • in the four marked positions between the I/O cabinet and the power cabinet on the right side of the I/O cabinet.

    From Power Cabinet to Power Cabinet

    From Power Cabinet on the Right Side of the I/O Cabinet to the I/O Cabinet

  18. Verify that the right-most power cabinet and the left-most power cabinet for the I/O cabinet has the covers (0M-98993 and 0M-82316) and the side panels installed before continuing.

    1500 kW I/O with Maximum Number of Power Cabinets

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.