990-5783L-001

Decommission or Move the UPS to a New Location

NOTE: Contact Schneider Electric for removal of the interconnection busbars between the cabinets.
  1. Shut down the UPS completely – follow the instructions in the UPS operation manual.
  2. Lockout/Tagout all disconnect devices in the switchgear in the OFF (open) position.
  3. Lockout/Tagout all battery disconnect devices in the switchgear/battery solution in the OFF (open) position.
  4. Open the front door of the UPS.
  5. If present, Lockout/Tagout the backfeed disconnect device BF2 in the OFF (open) position.
  6. Open the front door of the I/O cabinet and the power cabinets.
  7. Remove the two metal plates from the I/O cabinet.
  8. Measure for and verify ABSENCE of voltage on each input/bypass/output/DC busbar before continuing.
    DANGER
    hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Measure for and verify ABSENCE of voltage on each input/bypass/output/DC busbar before proceeding.
    Failure to follow these instructions will result in death or serious injury.

    Front View of the I/O Cabinet
    Remove numbers

  9. Disconnect and remove all power cables from the I/O cabinet. See Connect the Power Cables in a 380 V, 400 V, 415, and 440 V System or Connect the Power Cables in a 480 V System for details.
  10. Disconnect and remove all signal cables from the I/O cabinet. See Signal Cables for details.
  11. Contact Schneider Electric for removal of the interconnection busbars between the cabinets. The interconnections busbars must only be removed by a Schneider Electric-certified field service representative or service partner.
  12. Remove the seismic front anchoring brackets from the cabinets. Save for reinstallation. See Mount the Front Anchoring Brackets for details.
  13. Remove the top baying brackets and interconnection screws from the cabinets. Release the cabinets from the rear anchoring brackets by loosening the bolts on the front of the cabinets. SeePosition the Cabinets for details.
  14. Reinstall all removed plates and covers in the cabinets. See Final Mechanical Assembly of the I/O Cabinet and Final Mechanical Assembly of the Power Cabinets for details.
  15. Close and lock the front door of the cabinets.
  16. Raise the feet of the cabinets until the casters have full contact with the floor.
  17. You can now move each cabinet individually by rolling it over the floor on the casters.
    WARNING
    TIPPING hazard
    • The casters of the cabinet are exclusively for transport on flat, even, hard, and horizontal surfaces.
    • The casters of the cabinet are intended for transport over short distances (i.e. inside the same building).
    • Move at a slow pace and pay close attention on the floor conditions and the balance of the cabinet.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  18. Remove the rear anchoring brackets from the floor. Save for reinstallation. See Mount the Rear Anchoring Brackets for details.
  19. For transport over longer distances or in conditions that are not suitable for the casters of the cabinet:
    WARNING
    TIPPING hazard
    For transport over longer distances or in conditions that are not suitable for the casters of the UPS, ensure:
    • that personnel performing the transport have necessary skills and have received adequate training;
    • to use appropriate tools to safely lift and transport the cabinet;
    • to protect the product against damage by using appropriate protection (like wrapping or packaging).
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    WARNING
    Top-heavy cabinet
    The power cabinet is top-heavy. Take appropriate precautions during handling and preparation for transport/shipment.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

    Transportation requirements:

    • Mount the cabinet in a vertical position in the center of a suitable pallet. The pallet must be suitable for the weight of the cabinet. The I/O cabinet weighs 876 kg (1931 lbs). The power cabinet weighs 540 kg (1190 lbs).

    • Use appropriate means of fixation to mount the cabinet to the pallet.

    DANGER
    TIPPING hazard
    • The cabinet must be appropriately fixed to the pallet immediately after being placed on the pallet.
    • The fixation hardware must be strong enough to withstand vibrations and shocks during loading, transport, and unloading.
    Failure to follow these instructions will result in death or serious injury.
    WARNING
    Unexpected equipment behavior
    Do not lift the cabinet with a forklift/pallet truck directly on the frame as it may bend or damage the frame.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  20. Perform one of the following:
    • Decommission the cabinets, OR
    • Move the the I/O cabinet/power cabinet to a new location to install it.
  21. Only for installing the UPS in a new location: Follow the installation manual to install the I/O cabinet and power cabinets in the new location. See Installation Procedure for installation overview. Startup must only be performed by Schneider Electric.
    DANGER
    hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Startup must only be performed by Schneider Electric.
    Failure to follow these instructions will result in death or serious injury.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.