990-5783L-001

Connect the Emergency Power Off (EPO)

Do not connect any circuit to the EPO terminal block unless it can be confirmed that the circuit is Class 2/SELV.

All circuits connected must have the same 0 V reference.

The EPO input supports 24 VDC.

  1. Route the cables from your EPO through the top or bottom of the I/O cabinet and to the EPO terminals J4936–J4938 on 0P6547 as shown in Prepare for External Signal Cables.
  2. Connect the building EPO to the terminal block according to one of the options below.
    NOTE: Do not connect the terminal block to the board. Signal cables will be connected by Schneider Electric during the assembly service.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.