990-5783L-001

Torque Specifications

WARNING
Hazard of electric shock
All electrical connections must be torqued according to this table.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Bolt size

Torque

M6

5 Nm (3.69 lb-ft)

M8

17.5 Nm (12.91 lb-ft)

M10

30 Nm (22 lb-ft)

M12

50 Nm (36.87 lb-ft)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.