990-5783L-001

Route the PBUS Cables between Parallel UPS Units

NOTE: Do not connect the PBUS cables. PBUS cables will be connected by Schneider Electric during the assembly service.

Top Cable Entry Systems

Bottom Cable Entry Systems

  1. Route the PBUS cables from the installation kit 0H-0889 through either the top or the bottom of the I/O cabinet according to the principle below.
    NOTE: The PBUS 1 cables are white and the PBUS 2 cables are red.
    NOTE: The total length of the PBUS cables must not exceed 60 m (197 ft).

    Example of System with Three UPSs in Parallel

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.