Troubleshooting
| Problem description | Probable cause | Solutions |
|---|---|---|
| The operation LED blinks fast red after a HeatTag self-diagnostics. | Fan clogging detected in the HeatTag sensor. | Clean the fan air inlet (see detailed procedure). |
| The operation LED turns on red after a HeatTag self-diagnostics. | HeatTag sensor inoperative. | Replace the HeatTag sensor. |
Cleaning the HeatTag Fan Air Inlet
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Before maintaining the HeatTag sensor:
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
INOPERATIVE EQUIPMENT
Failure to follow these instructions can result in equipment damage.
|
Proceed as follows to clean the HeatTag fan air inlet with dry air duster:
-
Check that the tamper-seal tapes are not damaged. If the tamper-seal tapes are damaged or missing, contact your Schneider Electric local representative.
-
Disassemble the HeatTag sensor from the DIN rail.
- Put the HeatTag rear face on a flat surface, the HeatTag fan air inlet towards you.
-
Position the dray air duster vertically (spray nozzle to the top), 5 centimeters (1.97 in) away from the fan air inlet and spray dry air for 10 s on the fan air inlet.
-
Re-install the HeatTag sensor.
-
Switch on the HeatTag sensor.
-
Check that the HeatTag sensor is in normal operation (operation LED steady green).
-
If the problem persists, do the cleaning procedure again.
-
If the problem persists, replace the HeatTag sensor.
DANGER