DOCA0171EN-00

Unpairing the HeatTag Sensor

The HeatTag sensor has lost communication with the panel server or gateway for more than 15 minutes when:

  • The operation LED is green (blinking or steady).

  • The network status LED flashes red.

To manually unpair the HeatTag sensor:

  1. Press the operation button for more than 8 s.

  2. When the network status LED turns steady orange, release the button.

If you need to manually pair the HeatTag sensor to a panel server or gateway, see the corresponding procedure.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?