Hardware Description
Description
-
Operation LED
-
Network status LED
-
Operation button
-
QR code to access device information
-
DIN clip
-
Air inlet
-
Power supply connector
For information on installation, consult the instruction sheet available on the Schneider Electric website: MFR51738.
Operation LED
| LED indication | Description | Action |
|---|---|---|
| HeatTag sensor switched off. | None | |
| HeatTag sensor in test mode. | None | |
| HeatTag sensor in normal operation. | None | |
| HeatTag sensor has triggered an alert. | Investigate the cause of the heating in the switchboard. | |
| Minor malfunction detected. | Do maintenance operations on the HeatTag sensor (see Troubleshooting). | |
| Major malfunction detected. | Replace the HeatTag sensor. |
Network Status LED
QR Code
When the QR code on the front face of a HeatTag sensor is scanned with a smartphone running a QR code reader and connected to the Internet, the Go2SE landing page is displayed. The following information is available from the landing page:
-
HeatTag commercial reference and serial number
-
MAC address of the HeatTag IEEE 802.15.4 network
-
IEEE 802.15.4 installation code
-
HeatTag technical characteristics
-
HeatTag technical publications