DOCA0171EN-00

Manual Pairing of the HeatTag Sensor to a Panel Server or Gateway

The HeatTag sensor is not paired and can be manually paired to a panel server or gateway when:

  • The operation LED is green (blinking or steady).

  • The network status LED is steady orange.

To manually pair the HeatTag sensor 3 minutes after switching on:

  1. Press the operation button for less than 2 s.

    Result: The HeatTag sensor triggers the automatic discovery function of the gateway or panel server.

  2. The gateway or panel server discovers the wireless devices and pairs with the HeatTag sensor.

    Result:

    • The operation LED is green (blinking or steady).

    • The network status LED blinks green.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?