DOCA0171EN-00

Resetting the HeatTag Sensor to Factory Settings

The HeatTag sensor has lost communication with the panel server or gateway for more than 15 minutes when:

  • The operation LED is green (blinking or steady).

  • The network status LED flashes red.

To reset the HeatTag sensor to factory settings:

  1. Press the operation button for more than 8 s until the network status LED turns steady red.

  2. Release the button.

    Result: The network status LED turns steady orange (HeatTag sensor unpaired, with factory settings).

If you need to manually pair the HeatTag sensor to a panel server or gateway, see the corresponding procedure.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?