DOCA0171EN-00

Acknowledging an Alert

The HeatTag sensor has triggered an alert when :

  • The operation LED flashes orange.

  • The network status LED blinks green.

If the HeatTag sensor triggered an alert:

  1. Investigate the cause of the heating in the switchboard.

  2. Acknowledge the alert by pressing the operation button for less than 2 s.

    Result: The HeatTag sensor returns to normal operation mode when both the following conditions are met:

    • The operation LED turns to steady green.

    • The network status LED blinks green.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?