DOCA0171EN-00

Commissioning

When commissioned, the HeatTag sensor must be paired with Schneider Electric EcoStruxure panel servers or gateways. For detailed information about pairing the devices, see the user guide of the relevant panel server or gateway:

  • DOCA0172EN EcoStruxure Panel Server  - User Guide
  • DOCA0197EN PrismaSeT Wireless Panel Server - User Guide
  • DOCA0157EN PowerLogic PowerTag Link Gateway - User Guide

During the first 30 minutes after switching on the HeatTag sensor, the device is in test mode, that is , the operation LED blinks slowly green and the HeatTag sensor can trigger an overheating alert for test by using the HeatTag Tester or any other alert requested by panel server or gateway remotely. It takes another 8 hours for the HeatTag sensor to define its nominal environment and to be fully operational.
Each time the HeatTag sensor is powered on, 30 minutes and 8 hours sequences are repeated.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?