Automatic commissioning
- Connect toroid and turn on the power supply.NOTE: At first power up, the device performs automatic commissioning. You can connect from 1 to 12 toroids as per the requirement.
The device displays Detecting Toroid message with a percentage progress bar.
-
If toroid is detected, the Commissioning screen displays. An example of all 12 toroids connected and detected is as follows:
NOTE: If you have connected a toroid which is not one of the recommended toroids, then the device should be manually commissioned. See Manual commissioning. Refer to the Vigilohm catalog for the most up to date listing of compatible toroids. -
If toroid is not detected, the No Toroid message displays.
Perform one of the following action:
-
Check if the toroid is properly connected and navigate to . The device performs automatic commissioning.
-
The connected toroid is not one of the recommended toroids. The device should be manually commissioned. See Manual commissioning.
NOTE: Refer to the Vigilohm catalog for the most up to date listing of compatible toroids.
-
-
- You can check the wiring of the system. To check, see Checking wiring connection. If you do not want to check, ignore this step and continue to next step.
- Press
button.
The device exits the commissioning mode and displays Summary screen. An example of all 12 toroids connected and detected is as follows:
NOTE: The clock icon flashes to show that date and time needs to be set.NOTE:-
The device automatically exits commissioning mode after one hour if manual exit is not performed.
-
If you have connected a new toroid or replaced a toroid, navigate to . The device performs automatic commissioning.
-