7EN02-0422-01

Manual commissioning

The device must be manually commissioned if the connected toroid is not one of the recommended toroids.

NOTE: Refer to the Vigilohm catalog for the most up to date listing of compatible toroids.
  1. Navigate to Menu > Settings > Commissioning > Manual.

    The Manual screen displays the channel grid and a flashing dot on the channel 1 grid. This indicates the channel 1 is selected.

  2. Perform any one of the following:

    • To commission channel 1, press button.

    • To commission other channels, press button to navigate to the desired channel and press button.

    • To commission all channels, press button and press button.

    The Toroid Turns screen displays.

    For individual channel:

    For all channels:

  3. Press the button.

    The Toroid Turns screen displays the toroid turns value.

  4. Set the toroid turns (Allowed values: 300 to 3000) using the contextual menu buttons and .
  5. Press the button to save the toroid turns.

    A message Saved displays.

  6. Press Esc button.
    The Manual screen displays with the channel grid and a flashing dot on the channel 1 grid. This indicates the channel 1 is selected.
  7. Perform to for other non commissioned channels.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?