7EN02-0422-01

Setting date and time

Setting date and time ensures proper timestamps for the logs and trends.
  1. Press the flashing button.
    NOTE: The clock icon flashes to show that date and time needs to be set.

    The DATE/TIME screen displays.

  2. Set the date and time using the contextual menu buttons and .
  3. Press button to save the date and time.

    A message Saved displays.

    The Summary screen displays.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?