0614IB1802

Android—Configure ERMS Protection Settings

Example: Configure the ERMS protection settings using the EcoStruxure Power Device App (Android).

1. Press trip curve icon button.

2. Press “ERMS” button.

3. Press edit pencil.

4. Press anywhere on the protection settings.

5. Set protection settings to desired values.

6. Apply settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.