0614IB1802

Configure Using EcoStruxure Power Device App

The ERMS protection settings can be configured through the control unit’s Bluetooth link for both Android and iOS operating systems. In addition, the settings can be changed using a direct USB On The Go (OTG) link between an Android device and the control unit.

NOTE: ERMS settings cannot be changed when ERMS is engaged.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.