0614IB1802

Energy Reduction Maintenance Settings (ERMS) Engagement/Disengagement Using EcoStruxure Power Device App

The Energy Reduction Maintenance Settings (ERMS) function can be engaged/disengaged using the control unit’s Bluetooth link for both Android and iOS operating systems. In addition, ERMS can be engaged/disengaged via a direct USB OTG link between an Android device and the control unit.

NOTE: ERMS can be engaged/disengaged by only one smart device at a time.
NOTE: For Micrologic X control units with firmware versions < 3.0 and EcoStruxure Power Device App versions (Android > 3.0, iOS > 3.0), the Micrologic X firmware must be upgraded to version 3.0 or higher to be able to use the ERMS function.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.