0614IB1802

Primary Injection Testing

The ERMS function can be tested through primary injections means.

  • Use EcoStruxure Power Commission software to prepare the circuit breaker for primary injection testing.

  • The "Prepare for Primary Injection" button allows access to the "LSI Protection" and "Ground Fault Protection" functions.

These functions are used for:

  • LSI PROTECTION


    – Temporarily disable the ground fault function so that a single phase primary injected current can be applied without causing a Micrologic 6.0X control unit to trip on ground fault.

    – Reset the thermal memory of the circuit breaker so that the circuit breaker can be tested multiple times without the thermal memory function affecting the trip times.

  • GROUND FAULT PROTECTION
    Reset the thermal memory of the circuit breaker so that the circuit breaker can be tested multiple times without the thermal memory function affecting the trip times.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.