0614IB1802

Configure Using iOS Device

Example: Configure the ERMS protections settings using the EcoStruxure Power Device App (iOS).

1. Press trip curve icon button.

2. Press the “In = ...” arrow.

3. Press ERMS button.

4. Select “Configure”.

5. Set protection settings to desired values.

6. Apply settings.

QR code for this page

Was this helpful?