80459-641-01, Rev. 12

Appendix B–Non-Conductive Horizontal Bus Barrier Retrofit Kit

This appendix contains installation instructions for non-conductive horizontal bus barrier retrofit kits manufactured by Schneider Electric. These kits are for use in 15 in. (381 mm) and 20 in. (508 mm) deep Models 5 and 6 Motor Control Centers.

DANGER
Hazard of Electric Shock, Explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, CSA Z462, or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • After removing rivets and screws, verify that the compartment is free of loose particles.
  • Replace all devices, doors, and covers before turning on power to this equipment.
Failure to follow these instructions will result in death or serious injury.

Retrofit Kit Components

Remove Existing Components

Follow these instructions to remove the existing top horizontal wireway cover, bus barriers, units below the topshelf, and brackets (15 in. (381 mm) deep MCC):

Horizontal Wireway Cover

  1. Turn off all power supplying this equipment before working on or inside the equipment and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm power is off.

  2. Remove the screws that secure the top horizontal wireway cover to the structure, and then remove the cover.

Horizontal Bus Barriers

  1. Remove the screw located at the top of the two-piece bus barriers.

  2. Remove the screw located at the bottom of the two-piece bus barriers.

  3. Pull the two metal barriers out of the MCC and discard them.

Existing Brackets: 15 in. (381 mm) Deep MCC Only

If the MCC is 15 in. (381 mm) deep, use a 1/8 in. (3 mm) drill bit to remove the rivets that hold the right and left horizontal bus barrier brackets in place (see Remove Existing Brackets on the 15 in. (381 mm) Deep MCC). Discard the brackets after removal.

DANGER
Hazard of Electric Shock, Explosion, or Arc Flash
  • Drilling increases the chance of loose particles in the MCC.
  • Confirm that the compartment is free of loose particles before turning on power to this equipment.
Failure to follow these instructions will result in death or serious injury.

Remove Existing Brackets on the 15 in. (381 mm) Deep MCC

NOTE: Discard all retrofit brackets if the existing bus barrier bracket “B” (see Remove Existing Brackets on the 15 in. (381 mm) Deep MCC) is present on the 15 in. (381 mm) deep MCC. All holes are already present for direct mounting of the horizontal bus barrier.

Install the Retrofit Kit

Retrofit Brackets and Endcaps

Follow the applicable instructions below to install retrofit brackets into 15 in. (381 mm) or 20 in. (508 mm) deep MCCs. The top retrofit bracket must sit flush against the side channel. Slide the black grommets toward the back of the MCC.

  • 15 in. (381 mm) deep MCC: Use a rivet gun and two rivets in the retrofit kit to attach the retrofit brackets to the left and right-side channels (see 15 in. (381 mm) Deep MCC Retrofit Bracket).

    15 in. (381 mm) Deep MCC Retrofit Bracket

  • 20 in. (508 mm) deep MCC: Use the screws provided in the retrofit kit to attach the retrofit brackets to the left and right-side channels. Align the holes in the bracket and side channel as shown in 20 in. (508 mm) Deep MCC Retrofit Bracket.

    20 in. (508 mm) Deep MCC Retrofit Bracket

NOTE:
  • Even if the holes are present for a direct mounting of the endcap to the side channels, use the top retrofit bracket on 20 in. (508 mm) deep MCCs.

  • Before tightening the screws, push the bracket away from you so that the rear bracket hole is properly aligned with the side channel hole.

Follow the steps below to install the endcaps (see Endcap Placement).

Endcap Placement

  1. Rivet one endcap into place on the retrofit bracket or the side channel, either to the right or left side of the structure.

  2. Insert one end of the top track into the attached endcap.

  3. Place the other endcap on the opposite end of the top track and slide the top track into place.

  4. Rivet the second endcap to the retrofit bracket.

Bottom Track and Bottom Retrofit Bracket

  1. Using a 1/8 in. (3 mm) drill bit, drill out both rivets on the horizontal bus barrier bracket (the L-shaped bracket located on the topshelf (see Horizontal Bus Barrier (L-shaped) Bracket). Remove the bracket and discard it.

    Horizontal Bus Barrier (L-shaped) Bracket

  2. Install the bottom retrofit track (see Welded and Relay Topshelf Assemblies).

    • Welded topshelf: Align the holes of the shelf with those on the bottom track (see Welded and Relay Topshelf Assemblies). Rivet the track and the retrofit bracket to the topshelf.

      NOTE: If the bus contains four laminations, access the rivet holes from underneath the topshelf.

    • Relay topshelf: Align the two holes on the relay shelf with the bottom retrofit bracket holes (see Welded and Relay Topshelf Assemblies). Mark the places where you will drill other holes to secure the bottom track to the shelf. Drill the holes using a drill bit ranging from 0.136.–0.147 in. (3–4 mm) in diameter. Rivet the track and retrofit bracket to the topshelf.

      NOTE: The bottom retrofit track can be riveted directly onto the relay topshelf only if the relay assembly topshelf has two holes instead of four.

    Welded and Relay Topshelf Assemblies

    Welded Topshelf

    Relay Topshelf

Left and Right Panels

Installation

NOTE: The horizontal bus barrier contains two identical panels with arrows at the top. The “handle” on the left panel faces the front of the MCC section. The “handle cavity” on the right panel faces the front of the MCC section (see Right Panel (Side View)).

Right Panel (Side View)

Wireway Area

Horizontal Bus Area

  1. Align the arrows on the right panel and top track as shown in Installing the Right Panel into the Rear Groove.

    Installing the Right Panel into the Rear Groove

  2. Lift the panel up into the rear groove of the top track.

  3. Lower the panel into the rear groove of the bottom track.

  4. Slide the panel to the far right.

  5. Align the arrows on the left panel and top track.

  6. Repeat steps 2 and 3 using the left panel and front groove.

  7. Slide the panel to the left until it locks (snaps) into place.

  8. Verify that the barrier is completely closed by making sure that the wiring compartment is isolated from the bus compartment.

Removal (when required)

  1. With one hand, slide the left panel to the right until it unsnaps from the right panel.

  2. Align the arrows on the left panel and top track as shown in Aligning the Arrows on the Panels. Lift the panel out of the bottom track and remove the panel.

    Aligning the Arrows on the Panels

  3. Align the arrows on the right panel and top track as shown in Installing the Right Panel into the Rear Groove. Lift the panel out of the bottom track and remove the panel.

Replace Components

DANGER
Hazard of Electric Shock, Explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, CSA Z462, or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
Failure to follow these instructions will result in death or serious injury.

To replace the components of the MCC:

  1. Install the unit you removed in the section, Units Below the Topshelf. Refer to either the Model 5 MCC Installation and Maintenance Manual (8998IM9101) or Removing the Control Unit for instructions on installing units in an MCC.

  2. Replace the top horizontal wireway cover.

  3. Replace or close all other covers or doors before turning on the power to the MCC.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.