80459-641-01, Rev. 12

iMCC

This section includes instructions for the Model 6 Intelligent MCC (iMCC).

iMCC Overview

Model 6 iMCCs feature the same overall structure and unit features as Model 6 Motor Control Centers with additional “intelligent” capabilities. Two popular methods for configuring Model 6 iMCCs to customize your application are:

  • iMCC-Hardwired I/O: PLC Interwiring

  • iMCC-Network: Network Cabling

iMCC-Hardwired I/O: PLC Interwiring

This method offers a hardwired I/O system in the Model 6 MCC that provides basic information and control capabilities. With the I/O mounted in the MCC, the starters are wired to the I/O at the Schneider Electric manufacturing plant, and the system is tested prior to shipment.

iMCC-Network: Network Cabling

A key feature of our iMCC-Network solution is the integration of intelligent devices and device level networks for control and automation that delivers improved performance. Popular network protocols such as CANopen, DeviceNet™, Ethernet, Modbus, and PROFIBUS communicate directly to every unit of the iMCC for an effective method of connecting centralized control to widely distributed I/O.

Networking allows for easy monitoring of critical data of each motor or load connected to the iMCC, enabling precise process control. With this information, your staff can respond to potential problems proactively. Real-time access to information and records of last events allows for simplified diagnostics and reduced downtime.

The network cabling consists of a solution that is appropriate for your selected communication network. Our industry-leading, full-depth wireway effectively separates network cabling from high voltage cabling. Additionally, our standard wireway barrier isolates the communication cabling from the load cabling routed in the vertical wireway.

Networks/Communications Overview

iMCCs contain Schneider Electric devices with communication ports. Each device has a unique internal register map. These devices may be linked together to a single point.

The Schneider Electric publications listed in iMCC-related Literature may be useful in the setup, maintenance, and regular operation of your Model 6 iMCC. Upon request, your Schneider Electric field sales representative can provide them to you in print. Or, you can download these documents from the Schneider Electric Download Center: se.com/us/en/download/ .

Connecting the iMCC Cabling System

Units within iMCCs are connected at the factory. The cable used varies with the network type. The pin outs for the various networks are shown in Pin Outs for iMCC Networks.

Ethernet Networks use a Cat 5e RJ45 cable for connected devices.

NOTICE
LOSS OF COMMUNICATIONS
  • Do not use excessive force when making iMCC cabling connections.
  • Connections are keyed so that that pins are properly aligned.
Failure to follow these instructions can result in equipment damage.

Pin Outs for iMCC Networks

Network Cable Color
Blue White Red Black Bare
Modbus (two-wire RS-485) Signal + Signal - Not used Shield
PROFIBUS A (Neg) B (Pos)
DeviceNet CAN_L CAN_H V + V -
CANopen

Network Cabling

Factory supplied network cabling is installed in accordance with UL 845 procedures and practices and routed in the bottom horizontal wireway.

To make direct connections to Class 2 or Class CM systems, install Class 2 or Class CM wiring so that it is separated from power conductors either by a barrier or a minimum space of 0.25 in. (6 mm). Route power conductors in the top horizontal wireway for maximum separation.

External network cabling must comply with Class 2 or Class CM practices under the provisions of NEC Articles 725 and 800.

Cables Between Shipping Splits

Connect the trunk line cables between shipping splits by aligning the keyways and plugging the pin end of the trunk cable to the socket end of the next trunk cable. Screw the coupling ring until it is hand-tight. Repeat this process until all shipping splits are connected.

Load Cables

It is recommended to route all load cables in the top horizontal wireway to keep them isolated from the communications cabling. If you route the load cables in the bottom horizontal wireway, make sure to maintain a 0.25 in. (6 mm) distance between the communications cabling and all other cabling.

Communication Networks

There are three primary ways to connect communication networks: via bridges/repeaters, programmable logic controllers (PLCs), or a direct cable connection. Follow the applicable instructions below to make the cabling connections for your Model 6 iMCC.

Bridges/Repeaters

If the PLC is not in the local area of the MCC, you typically need to use a bridge/repeater to connect the communication network.

Terminating Resistors

For the communication network to operate properly, terminating resistors are required on each end of the network. If your iMCC is shipped with a bridge, repeater, and/or PLC, external terminal blocks (MCT485) are included with shipment.

Direct Cable Connection

To connect a cable directly to the network via the iMCC network cable:

  1. Determine which end (pin or socket) of the iMCC network you will attach to your cable.

  2. Strip back the communication cabling insulation.

  3. Based on the network, use the pin outs given in Network Connection Pin Outs.

Network Connection Pin Outs

Field Connection Termination Five-pin Socket/Pin
Modbus and PROFIBUS DeviceNet and CANopen
Pin # 1 Shield Shield
Pin # 2 Unused Red
Pin # 3 Unused Black
Pin # 4 White White
Pin # 5 Blue Blue

Typical Cabling Scheme for Modbus Two-wire

Orderable Item
in. (mm)

Part Number

Cap for unused pin end or tap

3463512-1

Cap for unused socket end or tap

3463512-3

Mini socket field attachable connector

5000129-287

Mini pin field attachable connector

5000129-292

20 (508) trunk extension

5000129-76

25 (635) trunk extension

5000129-78

30 (762) trunk extension

5000129-79

35 (889 trunk extension

5000129-80

25 (10.7) cable extension

5000129-81

NOTE: Shield must be grounded at one end only.

Typical Cabling Scheme for DeviceNet and CANopen (8A cable)

Orderable Item
in. (mm)

Part Number

Mini socket field attachable connector

1A5000-34DN

Mini pin field attachable connector

1A5006-34DN

25 (635) trunk cable

80420-919-01

30 (762) trunk cable

80420-920-01

35 (889) trunk cable

80420-921-01
NOTE: Shield must be grounded at one end only.

Typical Cabling Scheme for PROFIBUS

Orderable Item
in. (mm)

Part Number

Cap for unused pin end or tap 3463512-1
Cap for unused socket end or tap 3463512-3
20 (508) trunk extension 5000129-76
25 (635) trunk extension 5000129-78

30 (762) trunk extension

5000129-79

35 (889) trunk extension

5000129-80

25 (10.7) cable extension 5000129-81
NOTE: Shield must be grounded in all sections.

Operation

This section contains pre-operation checklists, energizing procedures, and remote and local programming procedures for TeSys T, TeSys Tera, and MotorLogic Plus motor protection relays, PowerLogic ION Meter, PowerLogic Power Meter, PowerLogic Circuit Monitor, Altivar drives, and Altistart soft starts.

Pre-operation Checklists

To verify that the iMCC is operating properly, complete both of the following checklists before energizing the equipment:

MCC Structure

  1. Complete the maintenance procedures beginning in Maintaining the MCC and continuing up to Insulation Test. This initial maintenance is necessary to detect any shipping damage or loose connections. Do not energize the MCC until initial maintenance is complete.

    NOTE: The following maintenance procedures are not necessary before energizing the MCC for the first time: Control Unit Removal, Stab Assemblies, Starter Contacts and Barriers/Insulators.
  2. Perform an insulation test on the MCC (see Insulation Test).

  3. If the MCC is equipped with ground fault protection, properly adjust, and test the ground fault protective device before energizing.

  4. Remove all blocks or other temporary holding means from the electrical devices.

  5. Remove any secondary shunt bars from the current transformers. Do not operate a current transformer with its secondary shunt bars open circuited.

  6. Manually exercise all switches, circuit breakers, and other operator mechanisms to help ensure that they are properly aligned and operate freely.

  7. Electrically exercise all electrically-operated switches, circuit breakers, and other mechanisms (but not under load) to help ensure that the devices operate properly. This may require an auxiliary source of control power.

  8. Verify proper interval and contact operation of the timers.

  9. Verify that overload relay FLA is set to proper application setting prior to operation.

  10. Verify that all load and remote-control connections have been made and that they agree with the wiring diagrams provided.

  11. Verify that all ground connections are made properly.

  12. Install the covers and close the doors; verify that they are all properly tightened.

iMCC Communications

NOTICE
LOSS OF COMMUNICATIONS
  • Do not use excessive force when making cabling connections.
  • Connections are keyed to help ensure that pins are properly aligned.
Failure to follow these instructions can result in equipment damage.

Before energizing the equipment, check the items below to verify that the iMCC networking and cabling are set up and connected properly:


  • Cabling Connections

  • Verify that the network length without a repeater is less than 1500 ft. (457 m).

  • Verify that the MCC cables are connected between shipping splits. See Cables Between Shipping Splits for instructions.

  • Verify that each device tap cable is properly connected to the main trunk line.

  • Verify that all network connections are secure.

  • Verify that terminating resistors are installed as required per network protocol.


Communications Setup

  • Verify that all devices have been assigned correct addresses; see Device Addressing for specific addressing parameters.

Energizing the MCC

DANGER
Hazard of Electric Shock, Explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, CSA Z462, or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
  • Review the Pre-operation Checklists, and verify that all items check out.
Failure to follow these instructions will result in death or serious injury.

To energize the MCC:

  1. Review the Pre-operation Checklists before energizing.

  2. Turn off all downstream loads, including distribution equipment and other devices that are remote from the MCC.

  3. Verify that all barriers, doors, and covers are closed before energizing the equipment.

  4. Energize the equipment in sequence, starting with the main, the feeder units next, and then the motor starter units.

  5. With all barriers in place and all unit doors closed and latched, turn on the units with a firm, positive motion.

  6. After all disconnect devices are closed, you may energize loads such as lighting circuits, starters, contactors, heaters, and motors.

MotorLogic Plus Local Programming

DANGER
HAZARd of electric shock, explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, CSA Z462, or local equivalent.
  • Turn off all power supplying this equipment before working on or inside the Motor Control Center.
  • Use a properly rated voltage sensing device to confirm that all power is off. Control units must be de-energized before performing maintenance on the MCC.
  • The unit disconnect switch must be locked in the off position before working on equipment.
Failure to follow these instructions will result in death or serious injury.

Local programming can be used for MotorLogic Plus setpoint programming and detected error readout purposes:

  1. Verify that the display is unlocked (the default setting) and disconnect all power.

  2. Turn off all power supplying this equipment before working on or inside the equipment and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.

  3. Connect a nine V supply to the “P” and “G” terminals using the supplied connector, Schneider Electric PN 80445-519-50 (see MotorLogic Plus Communication Module Terminals).

    MotorLogic Plus Communication Module Terminals

  4. Turn the “Mode Select” switch to the parameter you are programming. Refer to Schneider Electric instruction bulletin 30072-013-98 (see iMCC-related Literature) for a list of parameters.

  5. Press and hold the “Reset/Program” button.

    NOTE: The display does not illuminate for local programming if the “Mode Select” switch is in the “Run” position.
  6. Turn the “Display/Program” dial to the desired setting as shown on the LED display.

  7. Release the “Reset/Program” button.

  8. Turn the “Mode Select” switch back to the “Run” position.

  9. Disconnect the nine V supply and its connector.

Messages are displayed on the three-digit LED display when harmful conditions are detected. Local Message Display contains a list of the message codes and their definitions.

Local Message Display

Displayed Message Meaning
oc Tripped on over current
SP Tripped on single phasing
ub Tripped on voltage or current unbalance
uC Tripped on under current
cF Tripped on contactor misoperation
GrF Tripped on ground fault
HI Tripped on over-voltage
Lo Tripped on under-voltage
rP Incoming phases have been reversed
oFF A stop command was issued from a remote source

MotorLogic Plus Remote Programming

Remote programming can be used for setpoint programming and data acquisition purposes. Follow the steps below to remotely configure the MotorLogic Plus overload. (See Command Line Codes for a description of the command line codes referenced in the steps.)

  1. Stop the overload by sending code “02H” to the command register (C6H).

  2. If network programming has not been enabled, send code “05H” to the command register.

  3. Program the appropriate parameter. See MotorLogic Plus Address Descriptions (Read only, all registers are 16-bit words) for a register map with a list of parameters. For more detailed information, refer to Schneider Electric instruction bulletin 30072-013-102. See Read-Only Registers and Read/Write Registers to determine the location and addressing of parameters within the MotorLogic Plus register map.

  4. Restart the overload by using code “01H.”

Command Line Codes

Code Command
01H Start/reset
02H Stop
03H Display lock
04H Display unlock
05H Network program enable
06H Network program disable
07H Network watchdog enable*
08H Network watchdog disable*

MotorLogic Plus Address Descriptions (Read only, all registers are 16-bit words)

Address Code Description Notes
RAM Relative*
A0 1A0 VOLTAV Average voltage L–L V~
A2 1A1 IAVE Raw average current A (x100, x10, x1), multiplied by scale factor
A4 1A2 VUB Voltage unbalance 0–100%
A6 1A3 IUB Current unbalance 0–100%
A8 1A4 PFANGLE Power factor angle Degrees
AA 1A5 CAPTY Thermal capacity remaining 0–100%
AC 1A6 GFC Ground fault current A (x100, x10, x1), multiplied by scale factor
AE 1A7 ERCODE/TRIPRN Real time event (RTE) and trip indicator (TI) 8-bit nibble-coded RTE; 8-bit coded TI
B0 1A8 FH Event history Event order: 4th, 3rd, 2nd, Last
B2 1A9 PID Manufacture year/model and scale 8-bit year; 8-bit ID and scale
B4 1AA VA-C Line voltage A–C V~
B6 1AB VB-C Line voltage B–C V~
B8 1AC VA-B Line voltage A–B V~
BA 1AD IC Raw current phase C A (x100, x10, x1), multiplied by scale factor
BC 1AE IB Raw current phase B A (x100, x10, x1), multiplied by scale factor
BE 1AF IA Raw current phase A A (x100, x10, x1), multiplied by scale factor
C0 1Bo RD1 Remaining restart delay RD1  
C2 1B1 RD2 Remaining restart delay RD2  
C4 1B2 RD3 Remaining restart delay RD3  
C6 1B3 COMLINE Command line code (address C6H) See Bus Connection Torque Values 12 (write only)
C8 1B4 Scale PowerLogic scale parameter (read only) 0, 1, 2; 16-bit signed word (2’s complement, read only)
CA 1B5 LV Under-voltage threshold 170 V~ to HV (600 V~ model; 450 V~ to HV)
CC 1B6 HV Over-voltage threshold LV to 528 V~ (600 V~ model; LV to 660 V~)
CE 1B7 VUB Voltage unbalance threshold 2–15%, or 999 (off)
D0 1B8 MULT Effective turns ratio Determined by model
D2 1B9 OC Overcurrent threshold Current range of SSOLR
D4 1BA UC Undercurrent threshold 0.5 x OC Min. to OC Max., Off
D6 1BB CUB Current unbalance threshold 2–25%, or 999 (off)
D8 1BC TC Overcurrent trip class 5, J5, 10, J10, 15, J15, 20, J20, 30, J30
(J = Jam protection is enabled)
DA 1BD RD1 Rapid cycle timer 2–500 s
DC 1BE RD2 Restart delay RD2 2–500 min.
DE 1BF RD3 Restart delay RD3 2–500 min.
E0 1C0 #RU Restarts after UC 0, 1, 2, 3, 4, A
E2 1C1 #RF Number of restarts 0, 1, oc1, 2, oc2, 3, oc3, 4, oc4, A, ocA
(0 = manual, A = continuous, oc = automatic restart after RD2 expires)
E4 1C2 UCTD Undercurrent trip delay 2–60 s
E6 1C3 GF Ground fault threshold 0.15 x OC Min. to 0.2 x OC Max., Off
E8 1C4 ADDR RS-485 secondary address 01–99

Read-Only Registers

RAM Address Relative Address* Code Description Notes
A0 1A0 VOLTAV Average voltage L-L Volts
A2 1A1 IAVE Raw average current A (x100, x10, x1), multiplied by scale factor
A4 1A2 VUB* Voltage unbalance 0–100%
A6 1A3 IUB* Current unbalance 0–100%
A8 1A4 PFANGLE* Power factor angle Degrees
AA 1A5 CAPTY* Thermal capacity remaining 0–100%
AC 1A6 GFC* Ground fault current A (x100, x10, x1), multiplied by scale factor
AE 1A7 ERCODE/TRIPRN Bit-real time messages and trip indicator Bit # TRIPRN ERCODE
0 Event lockout Under-voltage
1 Remote stop Over-voltage
2 Contactor event Unbalance voltage
3 Under current Under current
4 Over current Phase reversal
5 Ground fault Unbalance current
6 Current unbalance Single phase voltage > 25%
7 Current single phase > 50% unbalance Single phase current > 50%
B0 1A8 FH* NIBBLE_CODED -4 event history The four-event history is based on the following scheme:
16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1, where bits 1–4 = Last event, bits 5–8 = 2nd last event, bits 9–12 = 3rd last event, and bits 13–16 = 4th last event. These four bits indicate a hex value that corresponds to the following events:
1 Over-voltage
2 Under-voltage
3 N/A
4 Contactor misoperation
5 Phase reversal
6 Single phase
7 Ground fault
8 Current unbalance
9 Remote off command
10 Overcurrent
11 Undercurrent
B2 1A9 PID* Manufacture year, month, product type/scale 8-bit year, 4-bit month, 4-bit I/O and scale
B4 1AA VA-C Line voltage A–C Volts
B6 1AB VB-C Line voltage B–C Volts
B8 1AC VA-B Line voltage A–B Volts
BA 1AD IC Raw current phase C A (x100, x10, x1), multiplied by scale factor
BC 1AE IB Raw current phase B A (x100, x10, x1), multiplied by scale factor
BE 1AF IA Raw current phase A A (x100, x10, x1), multiplied by scale factor
C0 1B0 RD1* Remaining restart delay RD1 Seconds
C2 1B1 RD2* Remaining restart delay RD2 Seconds
C4 1B2 RD3* Remaining restart delay RD3 Seconds

Read/Write Registers

RAM Address Relative Address Code Description Range Default
C6 1B3 COM-LINE Command Line* Reset/run/stop, display lock, network configuration enable MotorLogic Plus Command Register (C6 hex)
01H Start/reset
02H Stop
03H Display lock
04H Display unlock
05H Network program enable
06H Network program disable
C8 1B4 Scale PowerLogic scale parameter 0, 1, 1–2; 16-bit signed word (2s complement, read only) Model dependent
CA 1B5 LV Low voltage threshold 170 V (450 V*) - HV setting 435
CC 1B6 HV Over-voltage threshold LV setting - 528 V (660 V*) 500
CE 1B7 VUB Voltage unbalance threshold 2–15% or 999% 5%
D0 1B8 MULT CT/turns effective ratio 1 or 10–200 1
D2 1B9 OC Overcurrent threshold OL current range Min. rating
D4 1BA UC Undercurrent threshold 0.5 x OC Min. to OC Max., Off 0.8 x OC Min.
D6 1BB CUB Current unbalance threshold 2–25% or 999% 6%
D8 1BC TC Overcurrent trip class 5, J5, 10, J10, 15, J15, 20, J20, 30, J30
(J = Jam protection is enabled)
5 5 decimal
J5 133 decimal
10 10 decimal
J10 138 decimal
15 15 decimal
J15 143 decimal
20 20 decimal
J20 148 decimal
30 30 decimal
J30 158 decimal
DA 1BD RD1 Rapid cycle timer 2–500 seconds 10
DC 1BE RD2 Restart delay all events except undercurrent 2–500 minutes 8
DE 1BF RD3 Restart delay after undercurrent 2–500 minutes 20
E0 1C0 #RU # Restarts after undercurrent 0, 1, 2, 3, 4, A (Automatic) RU Values
8.1 0–4 in decimal
8.2 A = 255 decimal
E2 1C1 #RF # Restarts all events except undercurrent 0, 1, oc1, 2, oc2, 3, oc3, 4, oc4, A, ocA
(0 = manual, A = continuous, oc = automatic restart after RD2 expires)
RF Values
0 1 decimal
1 2 decimal
oc1 3 decimal
2 4 decimal
oc2 5 decimal
3 6 decimal
oc3 7 decimal
4 8 decimal
oc4 9 decimal
A 10 decimal
ocA 11 decimal
E4 1C2 UCTD Undercurrent trip delay 2–60 seconds 5
E6 1C3 GF Ground fault current threshold (0.4) AOL current range or Off 0.15 x Min.
E8 1C4 ADDR RS-485 secondary address 01–99 1

TeSys T Motor Management Controller

The following describes MCC starter units equipped with the TeSys T Motor Management Controller. Read and understand the Safety Precautions before you install, adjust, or perform maintenance on these units. For full details about MCC installation, refer to Installing the MCC.

NEMA Rated Control Unit (TeSys T Modbus)

TeSys T Controllers

 

Modbus

DeviceNet

PROFIBUS

Ethernet

CANopen

 

TeSys T Retrofit Applications

DANGER
Hazard of Electric Shock, Explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, CSA Z462, or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
Failure to follow these instructions will result in death or serious injury.
NOTE: For retrofit applications, contact your local Schneider Electric representative for assistance. Schneider Electric assumes no responsibility for the design or implementation of retrofits unless contracted to perform them. See Schneider Electric data bulletin 8998DB1004 for upgrade of the MotorLogic Plus or MotorLogic Plus II solid state overload relay to the TeSys T motor management system.

Remove the starter from the unit to replace the overload (melting alloy/bi-metallic). See Removing the Control Unit.

Use terminal blocks (OEKTTBML) for two-speed applications requiring multiple passes to achieve the proper adjustment range.

Restrain looped load cabling between the TeSys T controller and the terminal block with wire ties (or the equivalent) when terminal kits are used.

On 600 V Size 1 applications, add a third wire tie between the circuit breaker and contactor near the contactor line lugs. Refer to instruction bulletin 30072-013-29 for additional information.

Use copper wire only on device power and control terminals. Conductors must be sized for 60°C (140°F) or 75°C (167°F) National Electrical Code® (NEC®) ratings.

Pressure wire terminals are suitable for single conductor wire sizes #24–14, solid or stranded. Two conductor wire size is #24–18. Terminal instruction labels are located adjacent to the terminal block or on the wireway door.

Applications Requiring Turns

There are some applications that require more than one wiring turn through the TeSys T controller:

  • All NEMA Size 4 applications require three passes through separately mounted current transformers (CTs) rated 300:5.

  • Certain two-speed constant or variable torque applications require two passes through the TeSys T conductor (CT) windows through which the motor leads must pass before being connected to the load terminals on the contactor (T1, T2, and T3). These two-speed constant or variable torque applications are for NEMA Size 1 (3/4 HP, 480 V) and all NEMA Size 2. By allowing multiple passes (turns) of the load leads through these CT windows, protection can be provided for motors with a full-load current lower than the specified operating range. Two passes of the load leads through each window effectively increase (by a multiple of two) the current that the TeSys T senses.

  • All three conductor windows must have the same number of passes, looped in the same direction, for the TeSys T to operate properly.

  • Begin passes from the load side of the TeSys T through the CT window, and return via the windows provided between the baseplate and the TeSys T. The final pass terminates on the load side of the contactor.

  • MCC units requiring multiple passes are factory supplied pre-looped with #14 wire and interposing terminal blocks.

TeSys T Local Programming

DANGER
Hazard of electric shock, explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, CSA Z462 or local equivalent.
  • Turn off all power supplying this equipment before working on or inside the Motor Control Center.
  • Always use a properly rated voltage sensing device to confirm that all power is off. Control units must be de-energized before performing maintenance on the MCC.
  • The unit disconnect switch must be locked in the “off” position before working on equipment.
Failure to follow these instructions will result in death or serious injury.

Use Local Programming for set point programming and detected error readout purposes. Configure the TeSys T by using SoMove software, or an HMI (display) to set the parameters.

The Parameter Settings Sheet (included with MCC order drawings) lists all the parameters that are by the factory specific to each device application. Any settings not shown on the Parameter Settings Sheet are retained at device default values. To return the TesSys T controller to its default settings, press and hold the Test / Reset button down for 16–20 seconds.

NOTE: The TeSys T requires power for configuration.

Configuring with HMI

The HMI may be supplied either as a unit-mounted option, or as a separate, handheld programming kit containing one HMI and one 3.3 ft. (1 m) connection cable.

  1. Connect the HMI to the TeSys T unit:

    1. If supplied as a unit-mounted option, the connection is made at the factory.

      or

    2. Connect the programming kit via the standard, unit-mounted RJ-45 port.
  2. Input Full Load Current (FLC):

    1. Using the HMI, go to Menu>Protection Settings>Thermal>Thermal Overload>FLC1

      NOTE: For additional details, refer to the TeSys T LTMCUF Control Operator Unit User Manual and the TeSys T LTMR Motor Management Controller User Guide specific to your network communication protocol. (See iMCC-related Literature for the document numbers.)

TeSys Tera Motor Management Controller

The following describes MCC starter units equipped with the TeSys Tera Motor Management Controller. Read and understand the Safety Precautions before you install, adjust, or perform maintenance on these units. For full details about MCC installation, refer to Installing the MCC.

TeSys Tera Controllers

 

Modbus

ProfiNet™

PROFIBUS

Ethernet

IEC61850  

Applications Requiring Turns

There are some applications that require more than one wiring turn through the TeSys Tera controller:

  • All NEMA Size 4 applications require one pass through the 3 amp Tera Sensor Module from the external current transformer (CT) secondary. CTs are rated 300:5.

  • All NEMA Size 5 applications require two passes through the 25 amp Tera Sensor Module from the external current transformer (CT) secondary. CTs are rated 300:5.

    • MCC units requiring secondary passes using an external CT are factory supplied pre-looped with #14 wire and interposing terminal blocks.

  • Certain two-speed constant or variable torque applications require two passes through the TeSys Tera conductor (CT) windows through which the motor leads must pass before being connected to the load terminals on the contactor (T1, T2, and T3). Two passes of the load leads through each window effectively increase (by a multiple of two) the current that the TeSys Tera senses. Verify that the low speed and high speed Full Load Amperages fall within Tera current sensing range.

  • All three conductor windows must have the same number of passes, looped in the same direction, for the TeSys Tera to operate properly.

  • Passes should begin from the load side of the TeSys Tera through the CT window. The final pass terminates on the load side of the contactor.

TeSys Tera Local Programming

DANGER
HAZARd of electric shock, explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, CSA Z462, or local equivalent.
  • Turn off all power supplying this equipment before working on or inside the Motor Control Center.
  • Use a properly rated voltage sensing device to confirm that all power is off. Control units must be de-energized before performing maintenance on the MCC.
  • The unit disconnect switch must be locked in the “off” position before working on equipment.
Failure to follow these instructions will result in death or serious injury.

Local Programming can be used for set point programming and detected error readout purposes. Configure the Tesys Tera by using SoMove software, or an HMI (display) to set the parameters.

The Parameter Settings Sheet (included with the final MCC order documentation) lists all the parameters that are by the factory specific to each device application. Any settings not shown on the Parameter Settings Sheet are retained at device default values. To return the TeSys Tera controller to its default settings, press and hold the Test / Reset button down for 16–20 seconds.

NOTE: The TeSys Tera requires power for configuration.

Configuring with HMI

The HMI may be supplied either as a unit-mounted option, or as a separate, handheld programming kit containing one HMI and one 3.3 ft. (1 m) connection cable.

  1. Connect the HMI to the TeSys Tera unit:

    1. If supplied as a unit-mounted option, the connection is made at the factory.

      or

    2. Connect the programming kit via the standard, unit mounted RJ-45 port.
  2. Input Full Load Current (FLC):

    1. Using the HMI, Log into "Admin" Mode: MENU > FIRST SETUP > SYSTEM SETTING > IFLC1.

      NOTE: For additional details, refer to the TeSys Tera Motor Management Controller User Guide and the TeSys Tera LTMTCUF Control Operator Unit User Manual specific to your network communication protocol. (See iMCC-related Literature for the document numbers.)

PowerLogic ION Meter

Instructions for programming the PowerLogic ION 9000 Series meters are contained in Schneider Electric instruction bulletin 7EN02-0390.

PowerLogic Power Meter Series 800, 5500, 8000

Instructions for performing local and remote programming for the Power Meter Series 800 are contained in Schneider Electric instruction bulletins 63230500-200 and 63230500-224 (see iMCC-related Literature).

Instructions for performing local and remote programing for the Power Meter Series 5500 are contained in Schneider Electric instruction bulletin HRB1684301.

Instructions for performing local and remote programing for the Power Meter Series 8000 are contained in Schneider Electric instruction bulletin 7EN02-0336.

PowerLogic Circuit Monitor

Instructions for performing local and remote programming for the Circuit Monitor 3000 or Circuit Monitor 4000 series are contained in Schneider Electric instruction bulletin 63230-400-204 or 63230-300-209, respectively (see iMCC-related Literature).

Altivar 61/71

Instructions for performing local setpoint programming are contained in Schneider Electric instruction bulletin atv71_Programming_Manual_en (see iMCC-related Literature).

Instructions for performing remote setpoint programming are contained in Schneider Electric instruction bulletin atv71_Parameters_en (see iMCC-related Literature).

Altivar 630/930

Instructions for performing local or remote programming for the Altivar 630 drive are contained in Schneider Electric instruction bulletin EAV64318 (see iMCC-related Literature).

Instructions for performing local or remote programming for the Altivar 930 drive are contained in Schneider Electric instruction bulletin NHA80757 (see iMCC-related Literature).

Altistart 48

Instructions for performing local or remote programming for the Altistart 48 soft starter are contained in Schneider Electric instruction bulletin 1623736, (see iMCC-related Literature).

Altivar 480

Instructions for performing local or remote programming for the Altivar 480 soft starter are contained in the Schneider Electric ATS480 communication instruction bulletins (see iMCC-related Literature).

PowerPacT Circuit Breakers with MicroLogic Trip Units

Instructions for performing local or remote programming of the MicroLogic trip unit parameters can be found in Schneider Electric instruction bulletin 48940-313-01,

Device Addressing

Ethernet-based networks use classless IPv4 addressing. Unless specified otherwise, MCC devices are assigned addresses in the 10.10.10.0/24 subnet starting from 10.10.10.2.

Serial-based networks follow the specific addressing rules of the protocol used. Details of these addressing rules can be found in Serial Device Addressing. Unless specified otherwise, MCC devices are assigned addresses starting from 2.

Serial Device Addressing

Protocol Maximum Number of Addressable Nodes Address Range Address to Avoid
Modbus 31 2–247 127
PROFIBUS 126 2–125 126
DeviceNet 64 2–62 63
CANopen 127 2–126 127

Software

Configurable software-such as PowerLogic System Manager Software, Ecoreach, or SoMove is available for communication with your intelligent Model 6 iMCC components. For setup, operating, and maintenance instructions, consult the user manual included with your software package.

Network Security

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
  • Change default passwords to help prevent unauthorized access to device settings and information.
  • Disable unused ports/services and default accounts, where possible, to minimize pathways for malicious attacks.
  • Place networked devices behind multiple layers of cyber defenses (such as firewalls, network segmentation, and network intrusion detection and protection).
  • Use cybersecurity best practices (for example: least privilege, separation of duties) to help prevent unauthorized exposure, loss, modification of data and logs, interruption of services, or unintended operation.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.