Overview

Internally Mounted Surge Protective Devices

Surgelogic Type IMA

Internally mounted surge protective devices are installed integrally to systems for service entrance and branch panel surge suppression. Internally mounted SPDs installed next to the supply bus provide maximum performance inside Square D systems. Built-in performance is the way to achieve cost effective power quality and continuous operation (especially important for critical power facilities).

US and Canadian UL Recognized as a Type 2 (or 1 with optional suffix in catalog number) SPD Component Assembly to UL 1449 and UL 1283 standards. Complies with requirements of NEC Article 285 (2017) and CSA C22.2 No. 8-M1986 as appropriate. Complies with UL 96A Master Label requirements for Lightning Protection Systems.

Feedback