Disconnect Switches and Circuit Breakers

Class 9422 / Refer to Catalog 9420CT9701

Additional Accessories

Alternate Mounting Kit

Channel/Flange

Support Kit

Auxiliary Lock Plate

Additional Accessories

Accessory

Description

Cat. No.

Alternate Mounting Kit

Permits mounting Class 9422 Type A1 or A2 handle mechanisms in enclosures with flange thickness of 16 gauge to 0.5 in.

9422AM2

Auxiliary Lock Plate

Auxiliary kit recommended for use with the Class 9422 Type A-1 flange handle to facilitate padlocking the handle in the “OFF” position. Primarily used when the handle is mounted on the center channel of a multi-door enclosure. Also in any case where the enclosure doors interfere with the normal padlock slot in the flange handle. Meets both the Automotive and NFPA 79 specifications.

9422L1

Special Lugs for
Disconnect Switches

Copper Lugs only—Specify Form Y157

Tin Plated Aluminum Lugs for 400 A Type TG Switch—Specify Form Y1572 (000–750 kcmil Cu/Al wire)

Anderson Type VCEL Compression Lugs—Specify Form Y1574
Exceptions: None of the 30 A or 60 A disconnect switches are available with compression lugs.

Operating Rods

Standard operating rod for use with Class 9422 variable depth mechanisms. Included as standard in each kit.

9422R1

Extra long operating rod for use with Class 9422 variable depth mechanisms. Can be used as a substitute for the standard rod included in each kit to increase the maximum mounting depth 7 in. (Two are required for Types ARR, RR, ART, RT, ATE, TE, ATF, TF).

9422R2

Feedback