LVPED508016EN–03

How to Maintain the Charging Mechanism

Functions

The charging mechanism is used to close the main contacts.

Degradation Factors

The factors which can cause degradation of the charging mechanism are the following:

  • Dusty or dirty environment

  • Shocks

  • Corrosive atmosphere

  • Idle for long periods of time

Potential Hazards

Performing regular maintenance on the charging mechanism can help to avoid the potential hazards and consequences listed in the following table.

Hazard

Consequence

Personal injury

Equipment damage

Charging mechanism is jammed.

Jammed mechanism

Preventive Action

The following table lists the preventive maintenance procedures to be performed to maintain the charging mechanism.

Maintenance program

Preventive action

Procedure

Basic end-user preventive maintenance

Operate the device manually and electrically.

Mechanism NII_1_1

Charge the device electrically with MCH gear motor.

Mechanism NII_1_2

Check the complete closing of the device poles.

Mechanism NII_1_3

Standard end-user preventive maintenance

Check the MCH gear motor charging time at 0.85 Un.

Mechanism NIII_2_1

Check the general condition of the mechanism.

Mechanism NIII_2_2

Manufacturer preventive maintenance

Check opening and closing forces.

Contact your Schneider Electric field service representative.

Clean and regrease the mechanism.

For more information, refer to Preventive Maintenance Programs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.