LVPED508016EN–03

How to Maintain Power Connections

Functions

WARNING
HAZARD OF HEAT GENERATION
Power connections must never use other material than copper or aluminum.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Power connections are the links between devices and electrical distribution systems (for example, busbars, cables). Connection terminals are used to make the links.

Degradation Factors

The factors which can cause degradation of the power connections are the following:

  • Vibration

  • Overheating

  • Incorrect tightening torque

  • Deteriorated washer

Potential Hazards

Performing regular maintenance on the power connections can help to avoid the potential hazards and consequences listed in the following table.

Hazard

Consequence

Personal injury

Equipment damage

Fire

Death or serious injury

Thermal dissipation due to insufficient tightening torque

Burning of the cable insulation

Preventive Action

The following table lists the preventive maintenance procedures to be performed to maintain the power connections of the device.

Maintenance program

Preventive action

Procedure

Standard end-user preventive maintenance

Check connection system.

Power Connections NIII_2_1

For more information, refer to Preventive Maintenance Programs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.