Influence of Relative Humidity on Aging
Relative Humidity
|
Influence |
Appearance |
Consequences |
|---|---|---|
|
Corrosion of metal surfaces that is accelerated when a pollutant is present (for example, corrosive gas, salt, chlorine). |
Appearance of:
|
|
|
Deterioration of dielectric qualities of plastics. |
White traces on case |
Potential risk of a reduction in insulation |
|
Deterioration of electronic components, in particular SMCs and silver-coated components. This phenomenon is worsened by the presence of H2S corrosive gas (hydrogen sulphide). |
|
Short-circuiting of circuits resulting in non-operation of control unit protection, measurement, indication and communication functions |
|
Deterioration of electronic components, in particular non-varnished copper circuits. |
|
|
|
Degradation of opto-electronic components. |
– |
Potential failure of data transmission |
Recommendations
The maintenance and installation recommendations according to the relative humidity are defined in the following table:
|
Relative humidity |
Description |
Maintenance recommendations |
Installation recommendations |
|---|---|---|---|
|
≤ 70 % |
Level of relative humidity generally found in continental and temperate zones. The level is generally lower in switchboards due to the internal temperature rise. No significant deterioration is noted at this level. |
Preventive maintenance |
No particular recommendation |
|
70 % to 85 % |
Level of relative humidity generally found in zones close to water. Possible appearance of condensation on cold parts and accelerated rusting. |
|
No particular recommendation |
|
> 85 % |
|
|
Install heating resistors in the switchboard. |