LVPED508016EN–03

Manufacturer Preventive Maintenance Program

Definition

@TechPub writer (03/2019): FYI: Reminder: guide with the Manufacturer procedures (PSE1287) is released 12/2017. Not updated since for FWv2 or FWv3 projects.

The Manufacturer preventive maintenance program must be done exclusively by Schneider Electric field service representatives.

The Manufacturer preventive maintenance program includes the Basic and Standard end-user preventive maintenance programs.

The Manufacturer preventive maintenance program comprises:

  • Complete function checks.

  • Condition checks (test-based).

  • Complete part and system servicing (cleaning, greasing).

  • Control unit replacement (diagnostic-based).

The Manufacturer preventive maintenance program must be performed every five years in the case of normal operating conditions and user application with low criticality. Refer to the recommended frequency for the Manufacturer maintenance program for other cases.

Procedures

Part

Procedure title

Device

Measure insulation resistance

Mechanism

Check opening and closing forces

Clean and regrease the mechanism

Breaking unit

Measure the contact resistance for each pole

Auxiliaries

Preventively replace XF, MX, MN voltage releases (1)

Check opening time of MX opening voltage release

Check closing time of XF closing voltage release

Check opening time of MN undervoltage release

Control unit

Save protection settings, event histories (MicroLogic P and H) and create reports

Check continuity of the tripping chain by primary injection

Check integrated instantaneous protection (DIN/DINF) tripping

Check operation of MicroLogic thumbwheels

Preventively replace MicroLogic control unit and electrronic modules (2)

Chassis

Check connection/disconnection torque

Clean and regrease chassis of MasterPact drawout devices

Communication system

Check operation of the breaker communication module (BCM)

Check operation of the chassis communication module (CCM)

Check data transmission via communication bus

Mechanical interlocking

Operate mechanical interlocking by cable

Operate mechanical interlocking by rod

(1) As part of the preventive maintenance plan, Schneider Electric recommends replacing the voltage releases after 15 years of operation.

(2) As part of the preventive maintenance plan, Schneider Electric recommends that the field service representative replaces the MicroLogic control unit and associated M2C modules after 15 years of operation. Each time the MicroLogic control unit is replaced, the performer, and the rating and sensor plugs must be replaced by the field service representative.

Time Required

The average total time required for a Schneider Electric field service representative to perform this maintenance program including the Standard one, is as follows:

  • From 1.5 hours to 2 hours depending on the frame size, for a fixed device with all accessories installed.

  • From 2 hours to 3 hours depending on the frame size, for a drawout device with all accessories installed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.