Influence of Interrupted Currents on Aging
Interrupted Currents
|
Influence |
Appearance |
Consequences |
|---|---|---|
|
Wear of fixed and moving contacts |
Deterioration of contacts |
Beyond the electrical-endurance limit, device temperature rise increases due to the greater contact resistance and a reduction in the pressure of contacts. |
|
Wear of the arc chutes (insulating materials, separators) |
Deterioration of insulation |
Beyond the electrical-endurance limit, the insulation (input/output and between phases) is reduced, which results in a reduction of device suitability for isolation. In this case, the safety of persons is not guaranteed. |
Recommendations
The maintenance and installation recommendations according to the interrupted currents are defined in the following table:
|
Thresholds |
Description |
|---|---|
|
I/In ≤ 0.4 |
This level of interrupted current corresponds to the mechanical durability (see Mechanical endurance). |
|
I/In ≤ 0.8 |
This level of interrupted current corresponds to approximately 125 % of the electrical durability. |
|
I/In |
This level of interrupted current corresponds to the electrical durability at the specified voltage (see Electrical endurance). |