LVPED508016EN–03

How to Maintain the Main Contacts

Functions

A Fixed contact

B Movable contact

The main contacts of the device:

  • Are mounted in the arc chamber

  • Are composed of the fixed and the movable contacts

The movable contacts make (close) or break (open) the electrical circuit under normal conditions (at rated current In) or fault conditions (overload and short-circuit).

Degradation Factors

The factors which can cause degradation of the main contacts are the following:

  • Frequent switching operations at rated current

  • Stresses due to high short-circuit currents

Potential Hazards

Performing regular maintenance on the main contacts can help to avoid the potential hazards and consequences listed in the following table.

Hazard

Consequence

Personal injury

Equipment damage

Fire

Death or serious injury

Thermal dissipation due to high-resistance contact

Degradation of the breaking unit

Preventive Action

The following table lists the preventive maintenance procedures to be performed to maintain the main contacts of the device.

Maintenance program

Preventive action

Procedure

Standard end-user preventive maintenance

Check the condition of the breaking unit.

Breaking unit NIII_2_1

Manufacturer preventive maintenance

Measure the contact resistance for each pole.

Contact your Schneider Electric field service representative.

For more information, refer to Preventive Maintenance Programs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.