LVPED508016EN–03

How to Maintain the Chassis

Functions

The chassis mechanism is used to rack the device in and out.

The sliding connections between the chassis and device are made up of two parts: clusters and disconnecting contacts. Grease between the clusters and the disconnecting contacts facilitates the connection and avoids damaging the silver-coated surface by reducing the racking-in friction.

Chassis and system of racking in and out

Clusters and disconnecting contacts

Degradation Factors

The factors which can cause degradation of the chassis are the following:

  • Dusty environment

  • Shocks

  • Corrosive atmosphere

  • Idle for long periods of time

  • Incorrect operation

Potential Hazards

Performing regular maintenance on the chassis can help to avoid the potential hazards and consequences listed in the following table.

Hazard

Consequence

Personal injury

Equipment damage

Safety shutter malfunction

Electric shock

Device remains jammed in connected position.

Jammed operation of the device in the chassis (racking-in and racking-out)

Preventive Action

The following table lists the preventive maintenance procedures to be performed to maintain the chassis.

Maintenance program

Preventive action

Procedure

Basic end-user preventive maintenance

Check device racking operation.

Chassis NII_1_1

Standard end-user preventive maintenance

Check operation of safety shutters.

Chassis NIII_2_3

Clean chassis and check presence of grease on chassis.

Chassis NIII_2_1

Check disconnecting contact clusters.

Chassis NIII_2_2

Manufacturer preventive maintenance

Check connection/disconnection torque.

Contact your Schneider Electric field service representative.

Clean and regrease chassis of MasterPact NT/NW drawout devices.

For more information, refer to Preventive Maintenance Programs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.